Using a OM40007 and when debugging cant connect to target (LPC54018)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using a OM40007 and when debugging cant connect to target (LPC54018)

887 Views
jdwil31401
Contributor I

This is the error I get after clicking debug

 

jdwil31401_0-1625788221038.png

jdwil31401_1-1625788270942.pngjdwil31401_2-1625788311333.png

jdwil31401_3-1625788332357.png

I have no clue what I am doing wrong and have tried using the target reset button and the reset button on the target.

I was able to debug 1 time and when I did that the code was running and I didn't hit f8 yet and configured a pin the updated code without stoping the program, ever since I get this error any recommendations are welcomed.

 

Thank you

Tags (1)
0 Kudos
Reply
0 Replies