Hello, I am recently designing a communication system using the TWR-K21F120MA. I want to use the UART communication interface. But i have got some problem. I cannot find the receiver and transmitter of UART on the board. I need to use at least 2 UARTs for my project.
Hello Alice
Thank you so much for the reply. it is really helpful.
And i check the schematic of TWR-k21F120MA. Is there any possibility to use the UART0_RX,UART0_TX,UART1_TX and UART1_RX(A41-A44 of J4) in the following picture. I just want to wire the two UARTS with my device.
Hi Harrison,
If you only use the Tower demo board, do not change the board or add some other transmitter,
then only the A43-A44 can used on this board, please pay attention it is UART2, sorry on this board , the virtual serial port and UART on TWR-SER use the same UART port.
BR
Alice
Hello Harrison,
Maybe you need Tover System:Tower System Modular Development Board Platform|NXP ,
on the TWR-SER moduleSerial (USB, Ethernet, CAN, RS232/485) Tower System Module|NXP , there is a receiver and transmitter of UART , please see the schematic to check
whether it can meet you, I attached it for you . On the TWR-SER, there only one transmitter.
While on the TWR-K21F120MA board, there also another virtual serial port - J2, you can directly use it send/ receive data.
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------