Stuck at ResetISR function

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Stuck at ResetISR function

2,456件の閲覧回数
Nikolas_M
Contributor I

Hello all, 

I have yet to be able to upload to my MIMXRT685-AUD-EVK. 

I am trying to run any of the SDK examples, and every time I hit debug It throws me into the ResetISR function and I cannot step. If I try and set a breakpoint, it says "The debugger has set two breakpoints at the same address 0x[insert address]". In the debugger console it says "monitor exec SetRestartOnClose=1". 

Any help would be appreciated!

 

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,442件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi @Nikolas_M ,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To provide the fastest possible support, I'd highly recommend you refer to the post.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

1,798件の閲覧回数
yudeshui
Contributor II

Hi @jeremyzhou ,

I encountered the same issue now. Could you please share the post again to help me ?

Thanks in advance.

0 件の賞賛
返信