I'm trying to set up the ACMP for a LPC824 in MCUXpresso. When I select the positive and negative inputs in the analog comparator peripheral window, is shows that the inputs are disabled.
Here's what it says: ACMP_IN3 » [25] P3[16]/J5[2]/P0_14-ADC2-ACMP_I3, Disabled
The pins are routed in the PINS window.
How do I enable the pins to work with the ACMP?
Hi dporada
Please send me your demo project. I will check the problem directly.
Thanks
Jun Zhang
Hi dporada
I set the same ACMP pins and part as yours but it works well on my side.
I use SDK LPCXpresso824 v2.11, MCUXpresso IDE v11.6.1.
Please use the same version enviroment as above. Then follow attached steps in video to test again.
The project is also attached.
Thanks,
Jun Zhang
I have attached a screen shot of the Peripheral setup that has the Disabled lines.
This was not actually my problem. My problem was that the ACMP is not powered initially. I am surprised that the software that is used to configure the ACMP, initialize it, and set up the interrupts does not power it up. I did not see any mention in the documentation that this is required. I found the line of code in lpcxpresso824max_acomp_interrupt example that disables a bit that allows the ACMP to power up.
Did I miss something obvious?