Select COM-Port for programming/debugging in IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Select COM-Port for programming/debugging in IDE

2,944件の閲覧回数
steffenjahnkepa
Contributor III

Hello,

can someone tell me, how i choose the COM Port of the Board, that i want program/debug next. Unfortunately i cant find that config in the MCUXpressoIDE and getting tired of connect/unconnect the boards, if there are a lot of Boards in the Network, from USB-Ports. Thanks a lot!

ラベル(1)
タグ(2)
2 返答(返信)

2,587件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Steffen,

Which debug probe connection are you using (LinkServer, P&E, SEGGER)?

As a workaround, when moving from one board to another you could delete the current launch configuration files, this will force MCUXpresso IDE to perform a Debug Probe Discovery operation and present the list of debug probes found from which you can chose the new board.

pastedImage_1.png


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

2,587件の閲覧回数
steffenjahnkepa
Contributor III

Hello Carlos,

thanks for your response! Iam using the LinkServer debug probe connection. I already thought that this is the only way, but hoped for another easier :smileywink:. Thanks a lot!

Best Regards,

Steffen Jahnke