QN9090 debugging problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

QN9090 debugging problem

5,462件の閲覧回数
ljf1
Contributor I

When importing hello world program from SDK package, there is a problem that cannot be debugged, I would like to ask you about it

W@``RELS8%)H34I5$~B1S]J.pngW@``RELS8%)H34I5$~B1S]J.png

E:\MCUXpressoIDE\MCUXpressoIDE_11.3.1_5262\ide\plugins\com.nxp.mcuxpresso.tools.win32_11.3.0.202008311133 oolsinrm-none-eabi-gdb.exe: warning: Couldn't determine a path for the index cache directory.
GNU gdb (GNU Arm Embedded Toolchain 9-2020-q2-update) 8.3.1.20191211-git
Copyright (C) 2019 Free Software Foundation, Inc.
License GPLv3+: GNU GPL version 3 or later <http://gnu.org/licenses/gpl.html>
This is free software: you are free to change and redistribute it.
There is NO WARRANTY, to the extent permitted by law.
Type "show copying" and "show warranty" for details.
This GDB was configured as "--host=i686-w64-mingw32 --target=arm-none-eabi".
Type "show configuration" for configuration details.
For bug reporting instructions, please see:
<http://www.gnu.org/software/gdb/bugs/>.
Find the GDB manual and other documentation resources online at:
<http://www.gnu.org/software/gdb/documentation/>.

如需帮助,请键入“帮助”。
键入“apropos word”以搜索与“word”相关的命令。

程序已停止。
0x00002066 USART_ReadBlocking (base=0x4008b000, data=0x4015fb7 “”, length=1) 在 ../drivers/fsl_usart.c:441
441 而 (!(base->FIFOSTAT & USART_FIFOSTAT_RXNOTEMPTY_MASK))

临时断点 1,主断点 () 位于 ../source/hello_world.c:35
35 SYSCON->CODESECURITYPROT = 0x87654320;

 

0 件の賞賛
返信
8 返答(返信)

5,372件の閲覧回数
ljf1
Contributor I

它使用 SR150 和 QN9090 的 UWB 套件。请问除了QN9090之外,还有哪款芯片可以驱动SR150

0 件の賞賛
返信

5,395件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hello @ljf1

Hope you are doing well.

Could you please help us with your SDK version? Also, please consider updating your MCUXpresso IDE version.

Are you using a QN9090 Development Kit or is it a custom board? If you are using our QN9090 Dev Kit, please share your jumper configuration (a picture of the top side of your board would be very helpful).

Could you confirm that you have Python 3 installed on your system and added to the System variables PATH? You can consult the Getting Started with MCUXpresso SDK for QN9090, Section 3.3 Install Python3 for more information on this.

Regards,
Eduardo.

0 件の賞賛
返信

5,364件の閲覧回数
ljf1
Contributor I

It uses the UWB kit of SR150 and QN9090. May I ask which chip besides QN9090 can drive SR150

0 件の賞賛
返信

5,332件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

By any chance, are you using one of these Kits/Modules?

Regards,
Eduardo.

0 件の賞賛
返信

5,326件の閲覧回数
ljf1
Contributor I

Yes, I would like to ask if all chips containing SPI can drive the SR150 except for the QN9090?

0 件の賞賛
返信

5,317件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

You will need to redirect your questions to the Module Maker. Also, it is good to go with them to know the process and the support that they can provide you.

I apologize for the inconveniences this might cause you.

Regards,
Eduardo.

0 件の賞賛
返信

5,313件の閲覧回数
ljf1
Contributor I

Where is Module Maker? Can you provide the website?

0 件の賞賛
返信

5,299件の閲覧回数
EduardoZamora
NXP TechSupport
NXP TechSupport

Hi,

If you are using one of the Development Kits or Modules from our Partners (Trimension UWB Partners) you would need to go directly with them to know the process and the support that they can provide you, as the support path for this technology is through them.

For example:

Regards,
Eduardo.

0 件の賞賛
返信