MSCANDRIVER Questions

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MSCANDRIVER Questions

1,592件の閲覧回数
ljs20104
Contributor I

I am a s9keaz64amlh user.
I want to inquire about MSCAN.
I use 'MSCANDRIVER' provided by nxp.
CAN communication was confirmed.
So I try to do what I want, but I'm not good at it.

I try to run the motor when I get a certain CAN ID.
For example, I want to make a program where 0X81 is motor operation and 0X82 is motor reverse operation.
However, after writing the code as below, the specific CANID cannot be identified.

int main (void)
{
UINT8 err_status;

UINT32 a;

UINT8 data [7] = {6, 0, 0xff, 0, 0xff, 0, 0xff};
UINT8 Rdata [8];
UINT8 buffer_status [2];

Init_CAN (0, FAST);
Config_CAN_MB (0, 2, RXDF, 1);
GPIO_Init ();
Clk_Init ();
FAIL_APPLY ();
MSCAN_ModuleEn ();

    GPIOB_PDDR | = (1 << 16);
    GPIOB_PCOR = (1 << 16);

    EnableInterrupts;

    for (;;) {

    
    }
}

What should I modify in this code and how do I set a specific id?

I would appreciate it if you let me know.

if( a == 0x81){

 motor operation;

}

else if (a ==82){

 motor reverse operation;

}

I want to know a function or variable that sets a == 0x81 or 0x82.

0 件の賞賛
返信
1 返信

1,547件の閲覧回数
Alexis_A
NXP TechSupport
NXP TechSupport

Hi Jong,

To identify from where is received the CAN message one way could be to set a Mailbox with each ID that you mention, this could help you identify from which ID came the message.

Best Regards,
Alexis Andalon

0 件の賞賛
返信