MCUXpresso disables DWT counter when using trace

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MCUXpresso disables DWT counter when using trace

2,208 次查看
luizsantana
Contributor I

 

 

I'm using a MCUXpresso IDE v11.6.1, and a i.MXRT1021 using the SDK 2.11.0.

I'm using the DWT counter to count a few ticks for very brief delays. At the beginning of the code, I configure the counter.

 

    DWT->CYCCNT = 0;
    DWT->CTRL |= DWT_CTRL_CYCCNTENA_Msk;

 

I use the counter as 

 

__STATIC_FORCEINLINE __attribute((optimize("O3"))) void MiscTimeWaitPeriodNs( uint64_t p_timeoutNs )
{
    uint32_t nowTicks = DWT->CYCCNT;
    uint32_t lastTicks;
    float elapsedTicksSum = 0;
    float timeoutTicks = ( ((float)p_timeoutNs) * ((float)SystemCoreClock )) / 1000000000.0F;

    do
    {
        lastTicks = nowTicks;
        nowTicks = DWT->CYCCNT;
        elapsedTicksSum += nowTicks < lastTicks ?  nowTicks + (UINT32_MAX - (lastTicks - 1)) : nowTicks - lastTicks;
    } while ( elapsedTicksSum < timeoutTicks );
}

 

Everything works fine until I use the trace in the MCUXpresso IDE. When I start profiling, the IDE disables the DWT counter changing the state of the bit DWT_CTRL_CYCCNTENA_Pos in the DWT->CTRL. This change makes the counter DWT-.CYCCNT stops increasing. If I manually reanable this counter both the trace and the code works properly?

The MCUXpresso was supposed to change the state of this bit when I press play? 

 

0 项奖励
回复
4 回复数

2,166 次查看
luizsantana
Contributor I

My question is if the MCUXpresso should disable the counter when play the trace with the processor running. I didn't find any document saying this is supposed to happen. I attached a print of the console of the MCUXpresso where it says the counter has been disabled.

luizsantana_0-1666704167751.png

 

0 项奖励
回复

2,154 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I check the MCUXpresso console print info with below DWT_CTRL register setting:

0xE0001000 = 0x40010001

DWT_CTRL address is 0xE0001000, the CYCCNTENA bit is bit 0.

From the register setting, that should enable the CYCCNT.

Software sets DWT_CTRL.CYCCNTENA to 1 to enable the cycle counter.

That looks like the debugger console with incorrect message, should be enable the cycle counter.

Mike

0 项奖励
回复

2,150 次查看
luizsantana
Contributor I
Hi,

In the line just below, the console shows that
0xE0001000 = 0x40010000
It means the counter has been disabled in the end, and it remain disabled if I resume the code.
That looks the MCUXpresso sets DWT_CTRL.CYCCNTENA to 1 than cleans it when I play the button to start the trace.
0 项奖励
回复

2,170 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I checked the <ARM M7 Architecture Reference Manual>  with below description about DWT CYCCNT cycle counter and related timers:

CYCCNT is an optional free-running 32-bit cycle counter. When implemented and enabled, CYCCNT increments on each cycle of the processor clock. When the counter overflows it wraps to zero, transparently. CYCCNT does not increment when the processor is halted in Debug state.

From above description, I think you can enable CYCCNT cycle counter during the trace.

Mike

0 项奖励
回复