MCUXpresso & VSC Board Debug Issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso & VSC Board Debug Issue

31件の閲覧回数
Angel_OLG
Contributor II

Hello team, good day!

One customer is working with the RW612, to be more specific, with the IRIS uBlox Module. The customer reports the following issues:

  • MCUXpresso extension was import correctly to VSC - MCUXpresso SDK Repository Versión 25.9.0.

  • The example imported was the "frdmrw612_lpc_gpio_led_output" and modified for the uBlox evkit.
  • There was no error once the project was build.
  • The following error was shown, during the debugging session.

Angel_OLG_0-1756765203100.png

The project was detected on two different computers, and a similar project appears in MCUXpresso IDE (v25.6.136).

On the other hand, debug using the FRDM RW612 show the same errors, even though the customer completes the getting started using the MCU Link. 

Regards!

 

0 件の賞賛
返信
0 返答(返信)