MCUXpresso Pins Config Tool - View Pin Functions

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso Pins Config Tool - View Pin Functions

Jump to solution
4,295 Views
jeffthompson
Contributor V

In MCUXpresso Pins Config Tool, or in some other tool, can I view the functions available for a given pin? A configurator for a competing MCU supplier lets me look at the pin grid array and see the available functions for each each pin, but the NXP tool does not appear to have that capability, unless I'm missing something.

1 Solution
4,154 Views
BlackNight
NXP Employee
NXP Employee

Hi Jeff,

there are several options, showing hiere for a Kinetis device.

First if you move the mouse over a pin it shows the pin name which includes the functions:

pastedImage_1.png

If you click on a peripheral it shows which pins can be used for that function:

pastedImage_2.png

In the table view you get all the possible assignments for a pin. For example pin 28 can be GPIO, FTM Timer, UART, ....:

That's what you see in ohter tools as 'grid array', not sure if you have missed that one?

pastedImage_3.png

If you click on the checkbox, you get a list of possible assignments:

pastedImage_4.png

I hope this helps,

Erich

View solution in original post

3 Replies
4,155 Views
BlackNight
NXP Employee
NXP Employee

Hi Jeff,

there are several options, showing hiere for a Kinetis device.

First if you move the mouse over a pin it shows the pin name which includes the functions:

pastedImage_1.png

If you click on a peripheral it shows which pins can be used for that function:

pastedImage_2.png

In the table view you get all the possible assignments for a pin. For example pin 28 can be GPIO, FTM Timer, UART, ....:

That's what you see in ohter tools as 'grid array', not sure if you have missed that one?

pastedImage_3.png

If you click on the checkbox, you get a list of possible assignments:

pastedImage_4.png

I hope this helps,

Erich

4,151 Views
jeffthompson
Contributor V

Thanks, Erich. This really does help.

Jeff Thompson | Senior Electrical Engineer-Firmware

+1 704 752 6513 x1394

www.invue.com

0 Kudos
Reply
3,767 Views
fia1989
Contributor I

fia1989_0-1676955653981.png

Hi! When I open the pins tool, I get this but I can't select new pins. I had the window before but don't know how to access it. Please help!

0 Kudos
Reply