MCUXpresso Pins Config Tool - View Pin Functions

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MCUXpresso Pins Config Tool - View Pin Functions

跳至解决方案
4,231 次查看
jeffthompson
Contributor V

In MCUXpresso Pins Config Tool, or in some other tool, can I view the functions available for a given pin? A configurator for a competing MCU supplier lets me look at the pin grid array and see the available functions for each each pin, but the NXP tool does not appear to have that capability, unless I'm missing something.

标记 (1)
1 解答
4,090 次查看
BlackNight
NXP Employee
NXP Employee

Hi Jeff,

there are several options, showing hiere for a Kinetis device.

First if you move the mouse over a pin it shows the pin name which includes the functions:

pastedImage_1.png

If you click on a peripheral it shows which pins can be used for that function:

pastedImage_2.png

In the table view you get all the possible assignments for a pin. For example pin 28 can be GPIO, FTM Timer, UART, ....:

That's what you see in ohter tools as 'grid array', not sure if you have missed that one?

pastedImage_3.png

If you click on the checkbox, you get a list of possible assignments:

pastedImage_4.png

I hope this helps,

Erich

在原帖中查看解决方案

3 回复数
4,091 次查看
BlackNight
NXP Employee
NXP Employee

Hi Jeff,

there are several options, showing hiere for a Kinetis device.

First if you move the mouse over a pin it shows the pin name which includes the functions:

pastedImage_1.png

If you click on a peripheral it shows which pins can be used for that function:

pastedImage_2.png

In the table view you get all the possible assignments for a pin. For example pin 28 can be GPIO, FTM Timer, UART, ....:

That's what you see in ohter tools as 'grid array', not sure if you have missed that one?

pastedImage_3.png

If you click on the checkbox, you get a list of possible assignments:

pastedImage_4.png

I hope this helps,

Erich

4,087 次查看
jeffthompson
Contributor V

Thanks, Erich. This really does help.

Jeff Thompson | Senior Electrical Engineer-Firmware

+1 704 752 6513 x1394

www.invue.com

0 项奖励
回复
3,703 次查看
fia1989
Contributor I

fia1989_0-1676955653981.png

Hi! When I open the pins tool, I get this but I can't select new pins. I had the window before but don't know how to access it. Please help!

0 项奖励
回复