MCUXpresso IDE Without An Internet Connection

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE Without An Internet Connection

Jump to solution
5,258 Views
davethomas
Contributor I

I am trying to create a new project for the MK02FN128 using MCUXpresso IDE and a SDK generated using the online SDK builder. I've imported the SDK into the IDE and created a project, but I've found that I cannot use any of the Config Tools within the IDE -- I get an error message about not having the processor data, and that I should check my internet connection... This is a problem for me, because I don't typically have access to the internet on my development machine.

Is there a way to get the processor information into the IDE without an internet connection?

1 Solution
4,912 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Dave Thomas ,

I have reply you on your case of  salesforce , please check it .

And also I share it with here for some other customers need :

 

Outbound Email Message ~ Salesforce - Performance Edition

Please follow the below steps:

1. Export the related data from the PC with internet :

   From the menu of MCUXpresso IDE( or MCUXpresso Config Tools ): 

File->Export
-> Proceccor Data
-> Download Processor Data

  then choose the
chips you want to develop , and the download loacation .

After finish download ,
there will be two folder , "boards" and "prcossors",

2. Copy and paste to the PC without internet :

 - Manually copy (for example use flashdisk)  the above two folders to the PC you
want to use .

- Place them under
C:\ProgramData\NXP\mcu_data_v4, there are also

the two floder , please  put them in the corresponding place.

I also take a short video about the steps , while the download time is
so long , so just a simple demonstration on based on one PC.

 Please have a look
at my video. Hope it helps.
The video oversize the limits, so I upload it to google drive, please download it from here

https://drive.google.com/open?id=1ulnrHYJUcNqlBCl9neSsvPONABmYCnJS 

 

Alice

 -----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

3 Replies
4,913 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Dave Thomas ,

I have reply you on your case of  salesforce , please check it .

And also I share it with here for some other customers need :

 

Outbound Email Message ~ Salesforce - Performance Edition

Please follow the below steps:

1. Export the related data from the PC with internet :

   From the menu of MCUXpresso IDE( or MCUXpresso Config Tools ): 

File->Export
-> Proceccor Data
-> Download Processor Data

  then choose the
chips you want to develop , and the download loacation .

After finish download ,
there will be two folder , "boards" and "prcossors",

2. Copy and paste to the PC without internet :

 - Manually copy (for example use flashdisk)  the above two folders to the PC you
want to use .

- Place them under
C:\ProgramData\NXP\mcu_data_v4, there are also

the two floder , please  put them in the corresponding place.

I also take a short video about the steps , while the download time is
so long , so just a simple demonstration on based on one PC.

 Please have a look
at my video. Hope it helps.
The video oversize the limits, so I upload it to google drive, please download it from here

https://drive.google.com/open?id=1ulnrHYJUcNqlBCl9neSsvPONABmYCnJS 

 

Alice

 -----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

4,912 Views
davethomas
Contributor I

Thank you for your reply. This was initially not working for my existing project, but I found that upon recreating a project everything worked fine. Thanks again!

0 Kudos
Reply
4,913 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Dave,

Welcome!

BR

Alice

0 Kudos
Reply