Launching a JLink Debug encountered a problem

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Launching a JLink Debug encountered a problem

3,491件の閲覧回数
jqy
Contributor I

I have encountered a problem when I install the MCUXpresso IDE to my new windows 10 PC.

I finished the installation and imported my project, which was no problem before. When i tried to run the debug session, however, the IDE showed me an error message: Launching JLink Debug has encountered a problem. I went to the details: "Error in final launch sequence. Failed to execute MI command: -break-insert -t -f main".

And it also shows "Error message from debugger back end: Cannot access memory at address 0xab4"

If I restart the GDB server and launch debug first time. It showed "No source available for "0xfffffffe" 

 

Please help on this 

0 件の賞賛
返信
3 返答(返信)

3,079件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jiequiu,

Could you tell us which MCU and board are you using? Is your board using OpenSDA? Does the board works correctly on you old computer?

Thanks in advance!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信

3,079件の閲覧回数
jqy
Contributor I

Hi Carlos,

The IDE is working without any problem now! 

When I installed  the MCUXpresso IDE, I forgot to install the SDK and it gave me the issue. With the correct SDK, the IDE works fine.

Regards

Jieqiu

0 件の賞賛
返信

3,079件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Jiequiu,

 

It is good to hear it is now working correctly!

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信