LPC55S69 eval Board :SPI dma example Failed to transfer buffer !

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

LPC55S69 eval Board :SPI dma example Failed to transfer buffer !

4,953 次查看
sinda
Contributor I

Hi,

I'm testing SPI on new eval board LPC55S69, I'm trying to set this board as master with an external device , no one of examples provided by the SDK succeed to work ! is that related to peripheral tool which is not provided for this Device, or what?

 I'm using SPI7 with pins mentioned in photo attached , connected to  an external device set as slave! 

there is always error in SPI transfer like console photo shows !

0 项奖励
回复
5 回复数

4,836 次查看
sinda
Contributor I

Hi Sabina

I'm using the last SDK 2.6.2, I have two eval boards LPC55S69, I set one as slave with demo example (lpcxpresso55s69_spi_dma_b2b_transfer_slave) and the other one as a master with lpcxpresso55s69_spi_dma_b2b_transfer_master example, I ran the slave before then the master and the transfer fail as the console shows, I did not change anythings on both codes!

0 项奖励
回复

4,836 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

I've ran the examples without any modifications and had no problems.

Can you please check that the configuration of your connections are correct as shown in the readme file.

pastedImage_1.png

My results:

pastedImage_3.png

Best Regards,

Sabina

0 项奖励
回复

4,836 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello,

I'll be happy to help you in figuring out what is going on with your SPI communication. First can you please provide the SDK version you are using. Also can you provide the changes you made to the example to work with the SPI7, so I can try to reproduce the same error from my end.

Best Regards,

Sabina

0 项奖励
回复

2,545 次查看
Loïc
Contributor II

Hello @Sabina_Bruce ,

I have a similar problem. I'm using the SPI DMA example for the LPC55S69 as a Slave but I can't succeed answering to the master (SPI DMA Master LPC55S36).

I tried with the example without modification but nothing happens.

After that, I tried with a little bit of modification ( the communication is in the while and the master try to communicate with the slave  every loop) and I manage to have the MOSI working but not the MISO. It seems that the DMA Tx Slave doesn't work.

The slave code :

/*

* Copyright 2017 NXP

* All rights reserved.

*

*

* SPDX-License-Identifier: BSD-3-Clause

*/

 

#include "fsl_debug_console.h"

#include "fsl_device_registers.h"

#include "fsl_spi.h"

#include "fsl_spi_dma.h"

#include "fsl_dma.h"

#include "pin_mux.h"

#include "board.h"

#include <stdbool.h>

#include "fsl_power.h"

/*******************************************************************************

* Definitions

******************************************************************************/

#define EXAMPLE_SPI_SLAVE SPI8

#define EXAMPLE_SPI_SLAVE_IRQ LSPI_HS_IRQn

#define EXAMPLE_SPI_SSEL 1

#define EXAMPLE_DMA DMA0

#define EXAMPLE_SPI_SLAVE_RX_CHANNEL 2

#define EXAMPLE_SPI_SLAVE_TX_CHANNEL 3

#define EXAMPLE_SLAVE_SPI_SPOL kSPI_SpolActiveAllLow

#define TRANSFER_SIZE 4U /*! Transfer dataSize */

 

/*******************************************************************************

* Prototypes

******************************************************************************/

static void SPI_SlaveUserCallback(SPI_Type *base, spi_dma_handle_t *handle, status_t status, void *userData);

static void EXAMPLE_SlaveInit(void);

static void EXAMPLE_SlaveDMASetup(void);

static void EXAMPLE_SlaveStartDMATransfer(void);

static void EXAMPLE_TransferDataCheck(void);

 

/*******************************************************************************

* Variables

******************************************************************************/

uint8_t slaveRxData[TRANSFER_SIZE] = {0U};

uint8_t slaveTxData[TRANSFER_SIZE] = {0U};

 

dma_handle_t slaveTxHandle;

dma_handle_t slaveRxHandle;

 

spi_dma_handle_t slaveHandle;

 

volatile bool isTransferCompleted = false;

 

/*******************************************************************************

* Code

******************************************************************************/

static void SPI_SlaveUserCallback(SPI_Type *base, spi_dma_handle_t *handle, status_t status, void *userData)

{

if (status == kStatus_Success)

{

isTransferCompleted = true;

}

}

 

/*!

* @brief Main function

*/

int main(void)

{

/* Initialzie board setting. */

/* set BOD VBAT level to 1.65V */

POWER_SetBodVbatLevel(kPOWER_BodVbatLevel1650mv, kPOWER_BodHystLevel50mv, false);

/* attach 12 MHz clock to FLEXCOMM0 (debug console) */

CLOCK_AttachClk(BOARD_DEBUG_UART_CLK_ATTACH);

 

BOARD_InitBootPins();

BOARD_InitBootClocks();

BOARD_InitDebugConsole();

 

CLOCK_SetClkDiv(kCLOCK_DivPll0Clk, 0U, true);

CLOCK_SetClkDiv(kCLOCK_DivPll0Clk, 3U, false);

 

/* attach 50 MHz clock to HSLSPI */

CLOCK_AttachClk(kPLL0_DIV_to_HSLSPI);

 

/* reset FLEXCOMM for SPI */

RESET_PeripheralReset(kHSLSPI_RST_SHIFT_RSTn);

 

/* Print project information. */

PRINTF("This is SPI DMA transfer slave example.\r\n");

PRINTF("This example will communicate with another master SPI on the other board.\r\n");

PRINTF("Slave board is working...!\r\n");

 

/* Initialize the SPI slave instance. */

EXAMPLE_SlaveInit();

 

/* Configure DMA for slave SPI. */

EXAMPLE_SlaveDMASetup();

 

/* Start SPI DMA transfer. */

EXAMPLE_SlaveStartDMATransfer();

 

 

/* De-intialize the SPI instance. */

// SPI_Deinit(EXAMPLE_SPI_SLAVE);

 

while (1)

{

/* Waiting for transmission complete and check if all data matched. */

EXAMPLE_TransferDataCheck();

}

}

 

static void EXAMPLE_SlaveInit(void)

{

spi_slave_config_t slaveConfig;

 

/* Get default Slave configuration. */

SPI_SlaveGetDefaultConfig(&slaveConfig);

 

/* Initialize the SPI slave. */

slaveConfig.sselPol = (spi_spol_t)EXAMPLE_SLAVE_SPI_SPOL;

// slaveConfig.direction = kSPI_LsbFirst;

SPI_SlaveInit(EXAMPLE_SPI_SLAVE, &slaveConfig);

}

 

static void EXAMPLE_SlaveDMASetup(void)

{

/* DMA init */

DMA_Init(EXAMPLE_DMA);

 

/* configure channel/priority and create handle for TX and RX. */

DMA_EnableChannel(EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_TX_CHANNEL);

DMA_EnableChannel(EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_RX_CHANNEL);

DMA_SetChannelPriority(EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_TX_CHANNEL, kDMA_ChannelPriority0);

DMA_SetChannelPriority(EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_RX_CHANNEL, kDMA_ChannelPriority1);

DMA_CreateHandle(&slaveTxHandle, EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_TX_CHANNEL);

DMA_CreateHandle(&slaveRxHandle, EXAMPLE_DMA, EXAMPLE_SPI_SLAVE_RX_CHANNEL);

}

 

static void EXAMPLE_SlaveStartDMATransfer(void)

{

uint32_t i = 0U;

 

/* Initialzie the transfer data */

for (i = 0U; i < TRANSFER_SIZE; i++)

{

slaveTxData[i] = 0U;

slaveRxData[i] = 0U;

}

 

/* Create handle for slave instance. */

SPI_SlaveTransferCreateHandleDMA(EXAMPLE_SPI_SLAVE, &slaveHandle, SPI_SlaveUserCallback, NULL, &slaveTxHandle,

&slaveRxHandle);

 

}

 

static void EXAMPLE_TransferDataCheck(void)

{

static status_t state = kStatus_Success;

uint32_t i = 0U, errorCount = 0U;

spi_transfer_t slaveXfer;

static bool aborted = false;

 

 

/* Initialzie the transfer data */

for (i = 0U; i < TRANSFER_SIZE; i++)

{

if(state != kStatus_Success)

{

slaveTxData[i] = 0x55;

}

else

{

slaveTxData[i] = 0x88/*slaveRxData[i]*/;

}

}

 

slaveXfer.txData = (uint8_t *)&slaveTxData;

slaveXfer.rxData = (uint8_t *)&slaveRxData;

slaveXfer.dataSize = 2 * TRANSFER_SIZE * sizeof(slaveTxData[0]);

slaveXfer.configFlags = kSPI_FrameAssert;

 

/* Start transfer, when transmission complete, the SPI_SlaveUserCallback will be called. */

state = SPI_SlaveTransferDMA(EXAMPLE_SPI_SLAVE, &slaveHandle, &slaveXfer);

isTransferCompleted = false;

if (kStatus_Success != state)

{

PRINTF("There is an error when start SPI_SlaveTransferDMA \r\n");

SPI_MasterTransferAbortDMA(EXAMPLE_SPI_SLAVE, &slaveHandle);

aborted = true;

}

else

{

aborted = false;

}

if(!aborted)

{

/* Wait until transfer completed */

while (!isTransferCompleted)

{

}

isTransferCompleted = false;

 

PRINTF("\r\nThe transmitted data are now:");

for (i = 0; i < TRANSFER_SIZE; i++)

{

if ((i & 0x0FU) == 0U)

{

PRINTF("\r\n ");

}

PRINTF(" 0x%02X", slaveTxData[i]);

}

 

PRINTF("\r\nThe received data are now:");

/*Check if the data is right*/

for (i = 0; i < TRANSFER_SIZE; i++)

{

/* Print 16 numbers in a line */

if ((i & 0x0FU) == 0U)

{

PRINTF("\r\n ");

}

PRINTF(" 0x%02X", slaveRxData[i]);

/* Check if data matched. */

if (slaveTxData[i] != slaveRxData[i])

{

errorCount++;

}

}

if (errorCount == 0)

{

PRINTF("\r\nSPI transfer all data matched! \r\n");

}

else

{

PRINTF("\r\nError occurred in SPI transfer ! \r\n");

}

}

}

 I've tried a lot of thing but nothing works.

At one time, it was working, and the next day without any modification the code stopped working.

I am using SDK_2.16.000 for LPC55S69 (2024/07/12) and SDK_2.16.000 for LPC55S36 (2024/07/15).

@sindahave you found a solution to your problem ?

 

Best regards,

Loïc

标记 (5)
0 项奖励
回复

2,530 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hi @Loïc 

Kindly submit a new ticket so that it can flagged and assigned to an engineer. 

Best Regards,

Sabina

0 项奖励
回复