LPC55S69 Board, slave code in flash memory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55S69 Board, slave code in flash memory

1,177 Views
naga
Contributor III

Hi,

I use LPCXpresso55S69 and IDE V11.

Using the "New Project ..." command how to place the slave code in flash?

IDE forces slave code placement in RAM.

Neculai

0 Kudos
Reply
1 Reply

1,114 Views
Alexis_A
NXP TechSupport
NXP TechSupport

Dear Neculai,

 

The image of the slave code is placed in RAM but the primary code will boot the secondary core and place the image in flash. 

 

pastedImage_1.png

If you check the .map file you can see something like this that says where is loaded the slave core image.

 

I hope this helps you.

 

Best Regards,

Alexis Andalon

0 Kudos
Reply