Installing MCUXpresso on non-internet connected computer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Installing MCUXpresso on non-internet connected computer

1,144 次查看
joseph_lindula
Contributor IV

Hello, I need some help installing MCUXpresso on a computer that is not connected to the internet. I was able to download the installation file from my internet computer and install it on my non-internet computer. When I try to create a project I don't see any available devices. 

Are there any packages that I need to download and install?

 

Thank you

Joe

0 项奖励
回复
3 回复数

1,065 次查看
joseph_lindula
Contributor IV

Hello, I'm looking at using this device: LPC1112FDH28/102:5. 

0 项奖励
回复

1,045 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @joseph_lindula 

Please import lpcopen demo refer to the video in my attachment. 

If there is no LPCopen under MCUXpresso IDE installation directory. Please download from:

https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true 

Then copy it to your PC. Refer to the video in attachment to import demo and create new project.

If still have any issue, please contact me.

 

BR

Alice

0 项奖励
回复

1,118 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @joseph_lindula 

Which chip you use? 

There are two main categories of MCUs supported by MCUXpresso IDE. Preinstalled and via SDKs. Detail please refer to MCUXpresso IDE User Guide -> 4 Part support overview (preinstalled and via SDKs). 

 

BR

Alice

0 项奖励
回复