How to control UART0 with no printf or semiHosting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to control UART0 with no printf or semiHosting

2,699件の閲覧回数
claeskjellstrom
Contributor III

Regarding UART0 and how to control it in MCUXpresso IDE

Using MKE04, and both UART0 and UART1, UART1 is working but can't control UART0. 

Preprocessor:

__REDLIB__
SDK_OS_BAREMETAL
FSL_RTOS_BM
SDK_DEBUGCONSOLE=0
CR_INTEGER_PRINTF
PRINTF_FLOAT_ENABLE=0
CPU_MKE04Z64VLD4
CPU_MKE04Z64VLD4_cm0plus
__MCUXPRESSO
__USE_CMSIS
DEBUG

I have attached a screendump from the project.

Any sugesstions ?

/Claes

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,512件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi claes

If you do not need printf or semihosting, please change the SDK debug console from semihost console  to UART console.

Quick settings -> SDK Debug Console  -> UART console

pastedImage_1.png

Have a great day,
Daniel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

2,512件の閲覧回数
claeskjellstrom
Contributor III

Hi Daniel,

From what I can see now the situation is like this:

using redlib(none), initiating UART0 and UART1, I can control UART1 , regarding

UART0 I can read a char from UART0->D, but I can't send anything on Tx, I have checked that Tx and Rx are active.

/* UART0&1 init */
SIM->SCGC |= SIM_SCGC_UART0_MASK;
SIM->SCGC |= SIM_SCGC_UART1_MASK;

uart_config_t uart_config;
uart_config.baudRate_Bps = 19200U;
uart_config.parityMode = kUART_ParityDisabled;
uart_config.stopBitCount = kUART_OneStopBit;
uart_config.enableRx = true;
uart_config.enableTx = true;

UART_Init(UART0, &uart_config, 20000000U);
UART_Init(UART1, &uart_config, 20000000U);

When compiling for release I use None (-O0) and debug level(none) etc.......

When I simply changed through "quick setting" and UART Consol, the code size just increased but still same problem with UART0

From the pin_mux.c you can see

/* pin 23,24 is configured as UART0_TX, UART0_RX */
PORT_SetPinSelect(kPORT_UART0, kPORT_UART0_RXPTB0_TXPTB1);
/* pin 36,37 is configured as UART1_TX, UART1_RX */
PORT_SetPinSelect(kPORT_UART1, kPORT_UART1_RXPTC7_TXPTC6);
/* pin 43 is configured as RESET_b */
PORT_SetPinSelect(kPORT_RESET, kPORT_RST_RSTPE);
/* pin 44,42 is configured as SWD_DIO, SWD_CLK */
PORT_SetPinSelect(kPORT_SWDE, kPORT_SWDE_SWDE);

SIM->SOPT0 = ((SIM->SOPT0 &
/* Mask bits to zero which are setting */
(~(SIM_SOPT0_RXDFE_MASK | SIM_SOPT0_CLKOE_MASK)))

/* UART0 RxD Filter Select: 0x00u. */
| SIM_SOPT0_RXDFE(0x00u)

/* Bus Clock Output Enable: 0x00u. */
| SIM_SOPT0_CLKOE(0x00u));

Any other Ideas ??

Regards

Claes

0 件の賞賛
返信

2,512件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

HI Claes

I would suggest you refer to below link for information about printing with semihosting and printing with UART terminal

https://community.nxp.com/docs/DOC-334074 

Regards

Daniel

0 件の賞賛
返信