How do you disable the Welcome Page?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do you disable the Welcome Page?

Jump to solution
5,063 Views
w2vy
Contributor V

It is a simple enough question and in fact MCXU (10.3.0 2200) tells you this on the welcome page


MCUXpresso IDE

Disabling this Welcome Page

To disable the display of this page when running MCUXpresso IDE in future, untick...
  • Preferences -> MCUXpresso IDE -> General -> Show Welcome Page

Sadly there is no "Preferences" menu or submenu.

The Help file says the same thing


Chapter 3. IDE Overview

When MCUXpresso IDE is launched, a Welcome page is displayed (usually within the Editor view). This page contains product information including a link to the User Guide. If this page is not required on startup, it can be disabled via unticking the preference at Preferences -> MCUXpresso IDE -> General -> Show welcome view.

But the image above that tex shows a "Show Welcome Page" item

pastedImage_3.png

But clicking it does not seem to disable the welcome page

Any other suggestions?

It also seems that there are a few trivial bugs that can get fixed...

Tom

0 Kudos
Reply
1 Solution
4,970 Views
liborukropec
NXP Employee
NXP Employee

Hello Tom,

the global preferences are available from the main menu "Window | Preferences" (for Windows and Linux world. For Mac OS it is under the App name menu)

pastedImage_1.png

Regards,

Libor

View solution in original post

3 Replies
4,970 Views
w2vy
Contributor V

I hope they will still update the help files etc anyway!

Thanks!

0 Kudos
Reply
4,971 Views
liborukropec
NXP Employee
NXP Employee

Hello Tom,

the global preferences are available from the main menu "Window | Preferences" (for Windows and Linux world. For Mac OS it is under the App name menu)

pastedImage_1.png

Regards,

Libor

4,187 Views
BetoGreen
Contributor III
Its now in the lower right corner of the Welcome screen but if you wait too long it may change...

 

0 Kudos
Reply