Hello-World cannot connect to redlinkserver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello-World cannot connect to redlinkserver

Jump to solution
4,479 Views
lee2
Contributor II

Hello,

I am using the MCUXpresso IDE v11.2.0 and SDK 2.8.0 on the EVK-MIMXRT1064 board. I imported the hello_world example from the SDK. It builds all right without any errors or warnings. But when I try debugging it, I get the following error messages. I tried to restart the "redlinkserv.exe" several times by clicking the "Clean UP Debug" button but the results were the same. I screen captured the messages. Also, included is the .log file in the ~\workspace\.metadata.

Could you direct me how to resolve the issue?

Thank you very much in advance.

-Mike

Capture.PNGCapture2.PNGCapture3.PNGCapture4.PNG

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
4,416 Views
converse
Senior Contributor V

Looks like firewall is preventing the connection to redlinkserv. In your firewall settings, allow redlinkserv to accept connections.

Which version of Windows are you using?

View solution in original post

4 Replies
4,416 Views
lee2
Contributor II

You were right. Firewall was the culprit. Thank you so much.

0 Kudos
Reply
4,415 Views
lee2
Contributor II

Thank you for your reply. It make sense to me. I am using Windows 7 Professional. Is the OS supported?

0 Kudos
Reply
4,415 Views
converse
Senior Contributor V

Yes, the OS is supported. As I said, it looks like your firewall is preventing it from working. You need to change your firewall settings as described above.

4,417 Views
converse
Senior Contributor V

Looks like firewall is preventing the connection to redlinkserv. In your firewall settings, allow redlinkserv to accept connections.

Which version of Windows are you using?