Hello-World cannot connect to redlinkserver

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Hello-World cannot connect to redlinkserver

跳至解决方案
4,512 次查看
lee2
Contributor II

Hello,

I am using the MCUXpresso IDE v11.2.0 and SDK 2.8.0 on the EVK-MIMXRT1064 board. I imported the hello_world example from the SDK. It builds all right without any errors or warnings. But when I try debugging it, I get the following error messages. I tried to restart the "redlinkserv.exe" several times by clicking the "Clean UP Debug" button but the results were the same. I screen captured the messages. Also, included is the .log file in the ~\workspace\.metadata.

Could you direct me how to resolve the issue?

Thank you very much in advance.

-Mike

Capture.PNGCapture2.PNGCapture3.PNGCapture4.PNG

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
4,449 次查看
converse
Senior Contributor V

Looks like firewall is preventing the connection to redlinkserv. In your firewall settings, allow redlinkserv to accept connections.

Which version of Windows are you using?

在原帖中查看解决方案

4 回复数
4,449 次查看
lee2
Contributor II

You were right. Firewall was the culprit. Thank you so much.

0 项奖励
回复
4,448 次查看
lee2
Contributor II

Thank you for your reply. It make sense to me. I am using Windows 7 Professional. Is the OS supported?

0 项奖励
回复
4,448 次查看
converse
Senior Contributor V

Yes, the OS is supported. As I said, it looks like your firewall is preventing it from working. You need to change your firewall settings as described above.

4,450 次查看
converse
Senior Contributor V

Looks like firewall is preventing the connection to redlinkserv. In your firewall settings, allow redlinkserv to accept connections.

Which version of Windows are you using?