Flash & code usage analysis

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flash & code usage analysis

Jump to solution
2,467 Views
mspenard603
Contributor IV

Hi Gents,

 In MCUxpresso how can I get an idea of how much flash space is being used by the various parts of a codebase?

0 Kudos
Reply
1 Solution
2,398 Views
BlackNight
NXP Employee
NXP Employee

The MCUXpresso IDE V11 has the Image Info view which gives you exactly this information.

See New NXP MCUXpresso Eclipse IDE v11.0 | MCU on Eclipse 

Other than that, if you want to do it manually:

Listing Code and Data Size for each Source File with GNU and Eclipse | MCU on Eclipse 

I hope this helps,

Erich

View solution in original post

2 Replies
2,398 Views
mspenard603
Contributor IV

Wow, this new feature is fantastic.

0 Kudos
Reply
2,399 Views
BlackNight
NXP Employee
NXP Employee

The MCUXpresso IDE V11 has the Image Info view which gives you exactly this information.

See New NXP MCUXpresso Eclipse IDE v11.0 | MCU on Eclipse 

Other than that, if you want to do it manually:

Listing Code and Data Size for each Source File with GNU and Eclipse | MCU on Eclipse 

I hope this helps,

Erich