FXOS8700CQ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,923件の閲覧回数
amer_khawndi_se
Contributor I

Hi ,

 I want to make a  project using the FXOS8700CQ (Digital Motion Sensor) which is connected to FRDM K64F board and with MQX. Is there any driver code used to control and connect between the FXOS8700CQ and FRDM K64F board ?

Thanks,
Amer

0 件の賞賛
返信
1 解決策
1,856件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Amer, 

Within the SDK you will find an example of how to interface the FRDM-K64F with the Sensor Toolbox Development Boards for a 9-Axis Solution using FXAS21002C and FXOS8700CQ. You can download the SDK from the following link: Welcome | MCUXpresso SDK Builder 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,857件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Amer, 

Within the SDK you will find an example of how to interface the FRDM-K64F with the Sensor Toolbox Development Boards for a 9-Axis Solution using FXAS21002C and FXOS8700CQ. You can download the SDK from the following link: Welcome | MCUXpresso SDK Builder 

Have a great day,

Victor

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct"button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------- 

0 件の賞賛
返信