EA LPC4088 QSB examples

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EA LPC4088 QSB examples

9,487 次查看
pascalreygner
Contributor II

Bonjour,

I use Embedded Artist LPC4088 QSB card, but i do not find any library or example using it (this is not the same card than EA LPC4088 Dev. kit for which examples are provided).

Did someone already modify existing libraries to suite with thiscard?

thank you

标签 (1)
标记 (1)
0 项奖励
回复
9 回复数

8,797 次查看
pascalreygner
Contributor II

Hello,

it is now sure there are no examples for EA LPC4088 QSB card.

other idea : 

i have successufully imported my soft from mbed compiler to LPCXPRESSO but it did not compile, many errors occurs and i do not see solutions thus problems are various and never ends...

is their a solution to import correctly mbed compiler programm ?

best regards !

0 项奖励
回复

8,797 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Did you not see the pointer in my previous post to the LPCOpen example code that Embedded Artists make available on their website? https://community.nxp.com/thread/451585#comment-908392 

Regards,

MCUXpresso IDE Support

0 项奖励
回复

8,787 次查看
pascalreygner
Contributor II

Bonjour,

Yes i have seen it, and of course i have used it and made a complete application with those librairies and mbed complier.

But their are some troubles in some libraries (USB and Ethernet) and debug is really not easy.

So i have managed to import my complete soft in lpcxpresso to use a more pro debugger.

When i import a simple program compilation is correct and everything is working well.

But with a complex soft using mbed libraries, there are endless errors, and i do not succeed to compile my application.

I have used community remarks, this problem seems appearing, but i do not find solution at all.

If you have any guidelines for solving this it would be great.

The best solution would be to modifiy existing LPCXPRESSO libraries to make them working with my card (EA LPC4088 QSB).

But it is of course out of my capacities … ☹

If you know someone who can help me, for instance i did not found solution in community.

Thanks for your help.

Best regards.

Société TMS (Traffic Management & Services - SAS)

Pascal Reygner - Consultant

Web : www.tms-france.eu

+33 6 60 04 45 87

De : lpcxpresso_support

Envoyé : vendredi 26 mai 2017 13:17

À : Pascal REYGNER <pascal.reygner@tms-france.eu>

Objet : Re: - Re: EA LPC4088 QSB examples

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

Re: EA LPC4088 QSB examples

reply from LPCX support <https://community.nxp.com/people/lpcxpresso_support?et=watches.email.thread> in MCUXpresso Software and Tools - View the full discussion <https://community.nxp.com/message/909148?commentID=909148&et=watches.email.thread#comment-909148>

0 项奖励
回复

8,785 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Embedded Artists provide LPCOpen examples for this board on their website. See the DOCUMENTATION AND RESOURCES section of : LPC4088 QuickStart Board | Embedded Artists AB 

Regards,

MCUXpresso IDE Support

0 项奖励
回复

8,785 次查看
jeremyzhou
NXP Employee
NXP Employee
Thank you for your interest in NXP Semiconductor products and 
the opportunity to serve you.
Please download the library via the link below.

Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

8,786 次查看
pascalreygner
Contributor II

Bonjour,

Thank you for this answer, anyway i already dowloded this but didn’t find the good examples and libraires corresponding to EA LPC4088 QSB card.

Or may be i did not found it …

There are examples and libraries for a similar card (EA LPC4088 DEV KIT) which do not use same components (specially for ethernet link), thus libraries are not working.

Sincèrement.

Société TMS (Traffic Management & Services - SAS)

Pascal Reygner - Consultant

Web : www.tms-france.eu

+33 6 60 04 45 87

De : jeremyzhou

Envoyé : lundi 22 mai 2017 03:50

À : Pascal REYGNER <pascal.reygner@tms-france.eu>

Objet : Re: - Re: EA LPC4088 QSB examples

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

Re: EA LPC4088 QSB examples

reply from <https://community.nxp.com/people/jeremyzhou?et=watches.email.thread> jeremyzhou in MCUXpresso Software and Tools - <https://community.nxp.com/message/907357?commentID=907357&et=watches.email.thread#comment-907357> View the full discussion

0 项奖励
回复

8,786 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Pascal REYGNER,

Thanks for your reply.

After checking, there is no specific LPCOpen library for LPC4088 QSB.

Hope this is clear.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

8,786 次查看
pascalreygner
Contributor II

Bonjour,

This what i founded ☹.

Do you have aany idea how to work with it, or do you know someone who can help me for that ?

Sincèrement.

Société TMS (Traffic Management & Services - SAS)

Pascal Reygner - Consultant

Web : www.tms-france.eu

+33 6 60 04 45 87

De : jeremyzhou

Envoyé : lundi 22 mai 2017 09:08

À : Pascal REYGNER <pascal.reygner@tms-france.eu>

Objet : Re: - Re: EA LPC4088 QSB examples

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg> NXP Community

Re: EA LPC4088 QSB examples

reply from jeremyzhou <https://community.nxp.com/people/jeremyzhou?et=watches.email.thread> in MCUXpresso Software and Tools - View the full discussion <https://community.nxp.com/message/907424?commentID=907424&et=watches.email.thread#comment-907424>

0 项奖励
回复

8,786 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi Pascal REYGNER,

Thanks for your reply.

I think you need to do the manual migration work by yourself, and you can seek some suggestions from the community when you encounter some troubles.
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复