Duplicate Project in MCUXpresso 10.3

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Duplicate Project in MCUXpresso 10.3

ソリューションへジャンプ
2,665件の閲覧回数
mayursavaj
Contributor III

Recently we have Migrated to MCUXpresso 10.3. We have created One project also.

I have to replicate same project. So, I have created new workspace. using drag and drop method i have created new project. 

After changing only project name "Debug" option is not working. Find the below image for reference.

Before changing project Name:

pastedImage_1.png

After changed project Name

pastedImage_2.png

The issue is that after changes project name I unable to use "Debug" as its showing inactive and .axf file not creating.

Is there any setting missing?  where i have done wrong?

Please help me out to resolve this issue. 

Thanks in advance.

Regards,

Mayur Savaj

タグ(1)
0 件の賞賛
返信
1 解決策
2,529件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mayur Savaj,

Try to clean your project, then build again.

And when debug, use the Debug button in Quick Start , at the same time press Shift .

pastedImage_2.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,528件の閲覧回数
BlackNight
NXP Employee
NXP Employee

You need to change the debug configuration to point to the correct binary/project. Double-click on your .launch file in theproject, or use the menu Run > Debug Configuration, select your debug configuratinon and make sure it is pointing to the correct project and .axf file:

pastedImage_2.png

I hope this helps,

Erich

0 件の賞賛
返信
2,528件の閲覧回数
mayursavaj
Contributor III

Hi Erich Styger,

Thank you for your quick reply.

I did as per your guidance. It's shows same thing.

In Project explorer window ".axf" file is not displaying. But project location ".axf" file is created.

Is there any setting need to change?

Regard,

Mayur Savaj

0 件の賞賛
返信
2,530件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mayur Savaj,

Try to clean your project, then build again.

And when debug, use the Debug button in Quick Start , at the same time press Shift .

pastedImage_2.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------