Duplicate Project in MCUXpresso 10.3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Duplicate Project in MCUXpresso 10.3

Jump to solution
2,660 Views
mayursavaj
Contributor III

Recently we have Migrated to MCUXpresso 10.3. We have created One project also.

I have to replicate same project. So, I have created new workspace. using drag and drop method i have created new project. 

After changing only project name "Debug" option is not working. Find the below image for reference.

Before changing project Name:

pastedImage_1.png

After changed project Name

pastedImage_2.png

The issue is that after changes project name I unable to use "Debug" as its showing inactive and .axf file not creating.

Is there any setting missing?  where i have done wrong?

Please help me out to resolve this issue. 

Thanks in advance.

Regards,

Mayur Savaj

Tags (1)
0 Kudos
Reply
1 Solution
2,524 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mayur Savaj,

Try to clean your project, then build again.

And when debug, use the Debug button in Quick Start , at the same time press Shift .

pastedImage_2.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
2,523 Views
BlackNight
NXP Employee
NXP Employee

You need to change the debug configuration to point to the correct binary/project. Double-click on your .launch file in theproject, or use the menu Run > Debug Configuration, select your debug configuratinon and make sure it is pointing to the correct project and .axf file:

pastedImage_2.png

I hope this helps,

Erich

0 Kudos
Reply
2,523 Views
mayursavaj
Contributor III

Hi Erich Styger,

Thank you for your quick reply.

I did as per your guidance. It's shows same thing.

In Project explorer window ".axf" file is not displaying. But project location ".axf" file is created.

Is there any setting need to change?

Regard,

Mayur Savaj

0 Kudos
Reply
2,525 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Mayur Savaj,

Try to clean your project, then build again.

And when debug, use the Debug button in Quick Start , at the same time press Shift .

pastedImage_2.png


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------