Doubt regarding Timer in LPC804 Microcontroller

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Doubt regarding Timer in LPC804 Microcontroller

3,477 Views
VIGNESH_BABU
Contributor II

Hi,

I was worked in the development Board of LPC804 Micro controller.Where I have a confusion regarding how much of timers can we used in the LPC804 Microcontroller.

Below I was attached the images of user manual of LPC804 where they mentioned the one General purpose timer.

Next image denoted that in software where they mentioned 5 Timer Handler function.So please kindly

clear my confusion?

1]

User manual of LPC804User manual of LPC804

2]

Timer_Handler_FunctoinTimer_Handler_Functoin

0 Kudos
Reply
6 Replies

3,468 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi VIGNESH_BABU 

LPC804 only has one 32bit CTIMER.

Where is your code from? Is that NXP SDK demo code?

Thanks,

Jun Zhang

0 Kudos
Reply

3,462 Views
VIGNESH_BABU
Contributor II
Yes SDK example code for Timer.
0 Kudos
Reply

3,450 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Please send me the SDK version and demo full name. I will check,

0 Kudos
Reply

3,441 Views
VIGNESH_BABU
Contributor II

Here we attached the project file of SDK example of Timer in LPC804 Microcontroller.And I have one doubt regarding Timer.where I was unable to generate the time up-to 1 microsecond.Timer can generate up-to 300 microsecond.If I was gone above I was unable to get that time.Here I was attached the Images of DO(Digital Oscilloscope)

.Timer for 1 SecondTimer for 1 SecondTimer for 1 milisecondTimer for 1 milisecondTimer for 300 microsecondTimer for 300 microsecond  

0 Kudos
Reply

3,400 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Please let me know your demo code package download link and path. SDK version.

I will test the orinial code. Thanks.

0 Kudos
Reply

3,364 Views
VIGNESH_BABU
Contributor II

Thank you for your support

0 Kudos
Reply