Debugging with no flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debugging with no flash

1,614 Views
mspenard603
Contributor IV

Hi All,

 How do I properly debug with MCUxpresso and a J-Link on a iMXRT1062 without flashing first?  I've unchecked "Load Image". But when I click Debug, and then Restart, I don't ever hit any breakpoint I set in startup_mimxrt1062.c's init code. My Jlink must not be syncing even though it's attached or something...?

Untitled.png

0 Kudos
Reply
1 Reply

1,531 Views
FelipeGarcia
NXP Employee
NXP Employee

Hello Mike,

 

I recommend you to check this blog from a colleague Attaching to a Running Target with Segger J-Link, GDB and Eclipse | MCU on Eclipse 

 

I hope this helps!

 

Best regards,

Felipe

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored.

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

------------------------------------------------------------------------------ 

0 Kudos
Reply