Debugging on OM13087

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debugging on OM13087

1,377件の閲覧回数
luke_abela_16
Contributor I

I`m having an issue with regards to the OM13087 dev board containing the LPC 1115 - I am able to install the software and run the blink.c example code, however whenever I attempt to debug a second time after killing the first debug session, the IDE informs me it cannot locate any probes

"Linkserver is disconnected, not powered or in use"

I am attempted to debug using the CMSIS-dap debug probe. Upon removing and reinstalling the software, I encountered the same issue, any help would be appreciated.

タグ(2)
0 件の賞賛
返信
1 返信

1,316件の閲覧回数
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Luke,

Have you tried using the Clean-Up Debug button? It will kill all debug processes associated with LinkServer, P&E and
SEGGER debug connections. This button can be used in the event of a debugging crash to remove any failed processes that remain.

pastedImage_1.png


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 件の賞賛
返信