DEBUGGING PROBLEM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEBUGGING PROBLEM

3,720 Views
aravindpb5009
Contributor III

HAI

 

  I am trying to code LPC824 Microcontroller using MICUXPRESSO rev 10.3    during that debug time some problem i am facing when i debug some configuration errors are showing i searched in internet also in NXP community , ans downloaded many drivers but still i couldn't get positive result plz find my below attachment which it shown error  when i try to code to my microcontroller 

Labels (1)
0 Kudos
Reply
4 Replies

3,600 Views
danielchen
NXP TechSupport
NXP TechSupport

Hi Aravind:

I would suggest you delete the existing launch configuration, and the IDE will perform a probe discovery operation.

Please refer to below doc for more information

https://community.nxp.com/docs/DOC-335463 

Regards

Daniel

0 Kudos
Reply

3,600 Views
aravindpb5009
Contributor III

thanks for your assistance

0 Kudos
Reply

3,600 Views
berndsirozynski
Contributor III

Hello,
Sometimes i have the same problem with my LPC1768
to solve the problem i disconnect the USB and close the IDE.
after next start and conection the Debugprobe it works fine.

Bernd

0 Kudos
Reply

3,600 Views
aravindpb5009
Contributor III

ok i will try

0 Kudos
Reply