DEBUGGING PROBLEM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEBUGGING PROBLEM

3,722件の閲覧回数
aravindpb5009
Contributor III

HAI

 

  I am trying to code LPC824 Microcontroller using MICUXPRESSO rev 10.3    during that debug time some problem i am facing when i debug some configuration errors are showing i searched in internet also in NXP community , ans downloaded many drivers but still i couldn't get positive result plz find my below attachment which it shown error  when i try to code to my microcontroller 

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

3,602件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Aravind:

I would suggest you delete the existing launch configuration, and the IDE will perform a probe discovery operation.

Please refer to below doc for more information

https://community.nxp.com/docs/DOC-335463 

Regards

Daniel

0 件の賞賛
返信

3,602件の閲覧回数
aravindpb5009
Contributor III

thanks for your assistance

0 件の賞賛
返信

3,602件の閲覧回数
berndsirozynski
Contributor III

Hello,
Sometimes i have the same problem with my LPC1768
to solve the problem i disconnect the USB and close the IDE.
after next start and conection the Debugprobe it works fine.

Bernd

0 件の賞賛
返信

3,602件の閲覧回数
aravindpb5009
Contributor III

ok i will try

0 件の賞賛
返信