Custom command for the Speed setting

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Custom command for the Speed setting

2,327 次查看
sachin_singh
Fresh Out Contributor

Hi All,

I have the PN7462AU Eval kit, In which I need to develop the RF speed selection based on the user/custom command.

Through sending the command for respective speed will be gets activated. for example like if I send the RF 01 00 00 00 00 then 106 kbps should get selected, RF 02 00 00 00 00 then 212 kbps should get selected, RF 03 00 00 00 00 then 424 kbps should get selected and at RF 04 00 00 00 00 848 kbps should get selected.

So, Is there any need to resetting the RF field when request to change the speed, like if send for 212 speed from the 106 then it is require to reset the RF filed or not.

And using which API should I able to change the speed.

All the response & supports are highly appreciable ...!!!

Thanks in advance.

Regards

Manva

标签 (1)
0 项奖励
回复
1 回复

2,269 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

For this and any other further requests, please help us to contact your FAE or Distributor.

Have a nice day!

BR,

Ivan.

0 项奖励
回复