Can FRDM-K64F MCUXpresso IDE use Zephyr RTOS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can FRDM-K64F MCUXpresso IDE use Zephyr RTOS

1,897 Views
nicholas_yameen
Contributor II

Hi,

I have used Zephyr RTOS on the FRDM-K64F board mainly using the command line.  Is it possible to use MCUXpresso IDE to create a Zephyr project? I am using Ubuntu 16.04.

Thank you,

Nick

1 Reply

1,631 Views
maureen
NXP Employee
NXP Employee

Hi Nick,

You can generate an Eclipse project from cmake. This step needs to happen from the command line, but after that you can edit, build, and debug from Eclipse.

Here are some relevant links:

Application Development Primer — Zephyr Project Documentation 

Zephyr Project using Eclipse 

Maureen