CDT formatter: skip format section

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CDT formatter: skip format section

1,977件の閲覧回数
jordi_becares
Contributor III

Hi,

MCUxpresso formatter for C files doesn't support system to skip format section (like @formatter:off).

This feature is supported for java from a long time ago, and for CDT is supported from version 9.8 (see).

Last MCUxpresso version (v11.0.1_2563) has CDT v9.6.

When MCUxpresso will be upgrated to new CDT version?

Is there any workaround to support skip format section in current version?

Thanks

Jordi

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,873件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Yes, we have a new IDE version in the pipeline which integrates with a later version of Eclipse/CDT than we currently ship with in IDE v11.0.1.  This new IDE version is currently expected to be released around the end of the year.

In the meantime, maybe something like "cppstyle" might provide the functionality you are looking for. You can access this through the IDE's Help -> Eclipse Marketplace... menu, or at 

Regards,

MCUXpresso IDE Support

1,873件の閲覧回数
jordi_becares
Contributor III

Hi,

thanks for the feedback.

I checked the plugin, but it is not useful for my purpose.

I will wait for new release at the end of the year.

Regards

Jordi

0 件の賞賛
返信