C:\nxp\MCUXpressoIDE_10.2.1_795\ide\msys\bin\make.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

C:\nxp\MCUXpressoIDE_10.2.1_795\ide\msys\bin\make.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0

1,039 Views
leexiao
Contributor I

Hi, all

I have been using MCUXpressoIDE_10.2.1_795 for more than 6 months now. Previously, it worked quite well. However, from last week, when I try to clean or build a project I always got the error

"C:\nxp\MCUXpressoIDE_10.2.1_795\ide\msys\bin\make.exe: *** Couldn't reserve space for cygwin's heap, Win32 error 0"

I am using Windows 7 64 bit operating system.

I am very grateful if somebody can help me to solve this problem.

Regards.

Lee Xiao

0 Kudos
Reply
2 Replies

938 Views
converse
Senior Contributor V

See this thread

https://community.nxp.com/thread/456665 

[The fix is described in the User Guide]

0 Kudos
Reply

938 Views
BlackNight
NXP Employee
NXP Employee

Additionally, I recommend that you upgrade to the latest NXP MCUXpresso IDE v11, as this one has that dependency on Cygwin removed.

I hope this helps,

Erich

0 Kudos
Reply