BLDC motor control demo/example code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BLDC motor control demo/example code

3,543 Views
philocramer
Contributor I

I am trying to build a brushless DC motor controller. It would make my life a lot easier if I could see some demo/example code that does this. Can anyone help me please.
1) MCUXpresso IDE
2) LPCXpresso55S69 Board
3) lpc55S69 uP.
I suspect that the above doesn't exist, is there demo code for other eval boards?
Thanking you in advance.

0 Kudos
Reply
3 Replies

3,515 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @philocramer 

For BLDC motor control, we highly recommend you using MCXA153. Do not recommend using LPC55s69. 

There is application note you can refer to: 

https://www.nxp.com/webapp/sps/download/preDownload.jsp?render=true  

 

BR

Alice

0 Kudos
Reply

3,482 Views
philocramer
Contributor I

Thanks for the attempt, but that link is broken. I already have a bunch of application notes & library for BLDC. I was hoping that there exists some eval board that runs a brushless DC motor, so is there any eval board that has demo code for running a BLDC?

I do appreciate your efforts

Philo

0 Kudos
Reply

3,454 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @philocramer 

Yes, there is FRDM-MCXA153 board. 

https://www.nxp.com/design/design-center/development-boards-and-designs/general-purpose-mcus/frdm-de... 

Alice_Yang_4-1721962789297.png

 

And there is  BLDC motor control application note and code you can refer to. 

https://www.nxp.com/products/processors-and-microcontrollers/arm-microcontrollers/general-purpose-mc...  

Alice_Yang_3-1721962312381.png

 

BR

Alice

 

 

 
 

 

 

 

 

0 Kudos
Reply