lpc54606 no configuration tool for counter timer

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

lpc54606 no configuration tool for counter timer

1,038 Views
klausrenner
Contributor II

I'm trying to configure counter/timers on the LPC54606 using the configuration tool. I've tried both the configurator in MCUXpressoIDE_10.2.0_759 and the separate (older?) MCUxpresso Cofig V4.1 tool. None of the CTIMERs even show up in the peripheral list.  What's going on?

0 Kudos
Reply
1 Reply

845 Views
marek-trmac
NXP Employee
NXP Employee

Hi Klaus,

MCUXpresso IDE 10.2 and Config Tools V4.1 are based on the shared code-base and uses same data, so both tools support same set of devices and peripherals.

Peripherals Tools was introduced in Config Tools V4.0 and currently only subset of peripherals are supported, but they are incrementally added. Any update will be announced on community.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button
0 Kudos
Reply