install MCUXpresso_Config_Tools_v3_x64 fail( on windows 7 , x64, 12M RAM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

install MCUXpresso_Config_Tools_v3_x64 fail( on windows 7 , x64, 12M RAM

3,724 次查看
owenwang
Contributor I

Hi

When installing MCUXpresso Config Tools, errors occurs as below:

Server returned unexpected error 1624 attempting to install package c:\Users\wch0327\AppData\Roaming\NXP Semiconductors\MCUXpresso Config Tools 3.0.0.90\install\MCUXpresso_Config_Tools_v3_x64.msi

and fails to install this config tools.

Thanks

owen

0 项奖励
回复
3 回复数

3,349 次查看
owenwang
Contributor I

Sorry

Install on windows7, x64, 12G RAM

0 项奖励
回复

3,349 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello owen,

Could you please reinstall it , also download a new onw :

MCUXpresso Config Tools|NXP 

0 项奖励
回复

3,349 次查看
martinformanek-
NXP Employee
NXP Employee

Hello owen,

MCUXpresso Config Tools 3.0.0.90 is the version of MCUXpresso Config Tools 3.0.2, provided in the link.

to further investigate the issue we need the verbose log from the installation.

Could you please run the installer from command line and send us the log?

"MCUXpresso_Config_Tools_v4_x64.exe" /L*V "installation.log"‍‍

Thank you.

0 项奖励
回复