install MCUXpresso_Config_Tools_v3_x64 fail( on windows 7 , x64, 12M RAM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

install MCUXpresso_Config_Tools_v3_x64 fail( on windows 7 , x64, 12M RAM

3,718 Views
owenwang
Contributor I

Hi

When installing MCUXpresso Config Tools, errors occurs as below:

Server returned unexpected error 1624 attempting to install package c:\Users\wch0327\AppData\Roaming\NXP Semiconductors\MCUXpresso Config Tools 3.0.0.90\install\MCUXpresso_Config_Tools_v3_x64.msi

and fails to install this config tools.

Thanks

owen

0 Kudos
Reply
3 Replies

3,343 Views
owenwang
Contributor I

Sorry

Install on windows7, x64, 12G RAM

0 Kudos
Reply

3,343 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello owen,

Could you please reinstall it , also download a new onw :

MCUXpresso Config Tools|NXP 

0 Kudos
Reply

3,343 Views
martinformanek-
NXP Employee
NXP Employee

Hello owen,

MCUXpresso Config Tools 3.0.0.90 is the version of MCUXpresso Config Tools 3.0.2, provided in the link.

to further investigate the issue we need the verbose log from the installation.

Could you please run the installer from command line and send us the log?

"MCUXpresso_Config_Tools_v4_x64.exe" /L*V "installation.log"‍‍

Thank you.

0 Kudos
Reply