config tools v14 exports SDK example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

config tools v14 exports SDK example

ソリューションへジャンプ
3,239件の閲覧回数
shizj
Contributor III

I use config tools(v13.1-) to export SDK example(keil  project), but v14 seems not same.

How can I do it now or it's moved to another place?

thx!

タグ(1)
0 件の賞賛
返信
1 解決策
3,152件の閲覧回数
lukastyc
NXP Employee
NXP Employee

Hi,

It seems you are using the different product Config Tools for i.MX, that do NOT support clone(create standalone project) from SDK example.

Please use MCUXpresso Config Tools.

元の投稿で解決策を見る

3 返答(返信)
3,181件の閲覧回数
lukastyc
NXP Employee
NXP Employee

Hi,

Create a new configuration and project based on SDK example is on the same place in v13(v13.1) and v14.

lukastyc_0-1691400665155.pnglukastyc_1-1691400728468.png

Could you please provide us more details or screen shots about your issue?

Thank you

0 件の賞賛
返信
3,177件の閲覧回数
shizj
Contributor III

Thanks reply.

It looks difference with yours.

new.PNGversion.PNG

0 件の賞賛
返信
3,153件の閲覧回数
lukastyc
NXP Employee
NXP Employee

Hi,

It seems you are using the different product Config Tools for i.MX, that do NOT support clone(create standalone project) from SDK example.

Please use MCUXpresso Config Tools.