config tools v14 exports SDK example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

config tools v14 exports SDK example

Jump to solution
3,279 Views
shizj
Contributor III

I use config tools(v13.1-) to export SDK example(keil  project), but v14 seems not same.

How can I do it now or it's moved to another place?

thx!

Tags (1)
0 Kudos
Reply
1 Solution
3,192 Views
lukastyc
NXP Employee
NXP Employee

Hi,

It seems you are using the different product Config Tools for i.MX, that do NOT support clone(create standalone project) from SDK example.

Please use MCUXpresso Config Tools.

View solution in original post

3 Replies
3,221 Views
lukastyc
NXP Employee
NXP Employee

Hi,

Create a new configuration and project based on SDK example is on the same place in v13(v13.1) and v14.

lukastyc_0-1691400665155.pnglukastyc_1-1691400728468.png

Could you please provide us more details or screen shots about your issue?

Thank you

0 Kudos
Reply
3,217 Views
shizj
Contributor III

Thanks reply.

It looks difference with yours.

new.PNGversion.PNG

0 Kudos
Reply
3,193 Views
lukastyc
NXP Employee
NXP Employee

Hi,

It seems you are using the different product Config Tools for i.MX, that do NOT support clone(create standalone project) from SDK example.

Please use MCUXpresso Config Tools.