.axf File Loading problem using MCU xPresso

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

.axf File Loading problem using MCU xPresso

4,705件の閲覧回数
sreeramadhanala
Contributor I

Dear sir/Mam,

Now, we are migrating our application(MK22FN512VLH12)  to "MCU Xpresso10.2 V".

  1. In MCU xpresso , how to  load   " .axf" file(without project)  using "GUI Flash TOOL"  ?
  2. which are  the NXP / Third Party Debugger ports support ?(P&E Micro or J Link) please suggest if any? 

Thanks,

Dhanalakshmi s

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,931件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

New in MCUXpresso IDE version 10.2.0, the rearchitected GUI Flash tool provides flash
programming capabilities for all supported debug solutions.

pastedImage_1.png


For detail, see {MCUXpresso IDE 10.2.0 install folder}/MCUXpresso_IDE_User_Guide.pdf,
Chapter 13. The GUI Flash Tool.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,931件の閲覧回数
sreeramadhanala
Contributor I

Dear sir,

Thank you for your reply.

  1. Without any sample project  " GUI Flash Tool" is disabled  in "MCU xpresso " Tool bar.
  2. So , We are created a New Sample project .
  3. In  "GUI Flash Tool" ,browse our ".axf" file using File System option in "GUI Flash Tool'.
  4.  P&E Micro used  to Load the ".axf" File into "MK22FN512VLH12" flash.
  5. But , It shows the Following error.

   pastedImage_1.png

4.Please suggest me ,how to Load the ".axf" into  "MK22FN512VLH12" flash.

Thanks

Dhanalakshmi S

0 件の賞賛
返信

3,931件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I currently don't have K22 in hand. I tested K64 board with P&E OpenSDA interface.I didn't see any problem. See attached video

NOTE: Dummy project is necessary for using GUI Flash TOOL.


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信