Warning: Peripheral FLEXCOMM2 is not initialized

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Warning: Peripheral FLEXCOMM2 is not initialized

7,489件の閲覧回数
vijo
Contributor III

Hi,

Creating new configuration for processor LPC54606J512.

Selecting one of the signals in FC2 initiates the warning.

How and where to tell the config tool 4.1 about the initialization?

Checked the board LPCXpresso54618.mex which is using FC0-3 and 6,7.

No warnings for FC0-3 but warnings for FC6,7....

Thanks in advance.

0 件の賞賛
返信
6 返答(返信)

7,073件の閲覧回数
vijo
Contributor III

oops, paying attention to the peripheral tool solved the warning

0 件の賞賛
返信

7,073件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Viggo Joergensen,

After configure FC2, the code will be generated automatically in the file peripherals.c and peripherals.h.

Please take a screnshot about your warning and attached your config project .

BR

Alice

0 件の賞賛
返信

7,070件の閲覧回数
vijo
Contributor III

Hello Alice,

Still having warnings of a peripheral (ADC0) not initialized.

I’m using just one ad input – ch5.

Pls see the attached screen snips warning and routed pins.

Are you able to help ?

Thanks in advance.

Med venlig hilsen / Kind regards

Viggo Jørgensen

Civilingeniør, Software- / hardwareudvikler

Direkte: +45 87 12 51 09

E-mail: [email protected]<mailto:[email protected]>

<http://www.tarp.dk/nyheder/vi-stoetter-kampen-mod-brystkraeft.html>[www.tarp.dk]<http://www.tarp.dk/>

Fra: Alice_Yang <[email protected]>

Sendt: 2. august 2018 11:09

Til: Viggo Jørgensen <[email protected]>

Emne: You have been mentioned by Alice_Yang in Re: Warning: Peripheral FLEXCOMM2 is not initialized in NXP Community

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

You have been mentioned

by Alice_Yang<https://community.nxp.com/people/Alice_Yang?et=notification.mention> in Re: Warning: Peripheral FLEXCOMM2 is not initialized in NXP Community - View Alice_Yang's reference to you<https://community.nxp.com/message/1041420?commentID=1041420&et=notification.mention#comment-1041420>

0 件の賞賛
返信

7,070件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Viggo,

Please right click this warning, then choose "Initialize ADC0 peripheral":

pastedImage_1.png


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

7,070件の閲覧回数
vijo
Contributor III

Hello Alice,

Thanks for your quick response.

It solved the warning.

I wasn’t aware of the right click menu in that field.

Have a nice day too.

Med venlig hilsen / Kind regards

Viggo Jørgensen

Civilingeniør, Software- / hardwareudvikler

Direkte: +45 87 12 51 09

E-mail: [email protected]<mailto:[email protected]>

<http://www.tarp.dk/nyheder/vi-stoetter-kampen-mod-brystkraeft.html>[www.tarp.dk]<http://www.tarp.dk/>

Fra: Alice_Yang <[email protected]>

Sendt: 7. august 2018 11:59

Til: Viggo Jørgensen <[email protected]>

Emne: Re: - Re: Warning: Peripheral FLEXCOMM2 is not initialized

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Warning: Peripheral FLEXCOMM2 is not initialized

reply from Alice_Yang<https://community.nxp.com/people/Alice_Yang?et=watches.email.thread> in MCUXpresso Config Tools - View the full discussion<https://community.nxp.com/message/1043214?commentID=1043214&et=watches.email.thread#comment-1043214>

0 件の賞賛
返信

7,070件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

OK, welcome !


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信