Using clock tool code to switch between RUN and HSRUN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using clock tool code to switch between RUN and HSRUN

1,830 次查看
chriskeeser
Contributor III

I am trying to use the clock config tool to generate 2 clock configurations, a "HighPower" mode (run mode = HSRUN) and a "LowPower" mode (run mode = RUN).  My intent is to save power by switching back and forth between these two clock configurations depending on the processing needs. I have the 2 configurations set up in the MCUXpresso Config Tools, but when I observe the generated C source, the "LowPower" mode lacks code to switch the run mode back to RUN.  There is code in the "HighPower" mode to change the run mode to HSRUN, but if I switch back to "LowPower" the device will not be switched back to RUN.

Is this a bug in the tool?  A configuration error on my part?  A misuse of the tool?

I am using MCUXpress config tools v4.  Thanks for any insight.

0 项奖励
回复
1 回复

1,642 次查看
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Chris Keeser,

In my  opinion, the MCUXpresso Config tools for clock just configure

the run mode and clock mode , so it doesn't include the switch function from one mode to another,

we need change by our own code.

And about there is no configure in RUN mode(normal run state) on "LowPower",  because the default mode

after any reset is normal run state .

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复