USBHSD VCOM configuration for LPC55s69

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

USBHSD VCOM configuration for LPC55s69

1,833件の閲覧回数
Deeps_bang
Contributor III

Hi Team,

Development board:LPC55s69

SDK: SDK_2.x

i have to configure USB1 as VCOM.

so in MCU config tool peripheral setting , have used USBHSD peripheral .

Then used Device mode as required. 

And used preset :CDC VCOM(bare metal)

with this setting i initialized the peripheral .

when connected Hardware board , usb1 HS port detected ,

but when used serial terminal(Termite in my PC) for Communication , its not taking characters . the Serial window goes to hang state (unresponsive) as soon as I start to enter characters in serail window.

Is their any changes that I should do with code or peripheral settings to start communication with USB VCOM.???

 

regards,

Deep_Bang

 

 

 

 

0 件の賞賛
返信
2 返答(返信)

1,813件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Deeps_bang

Could you please specify which MCUXpresso SDK demo code + Demo board can reproduce your problem?

How to reproduce?

You have problem if input character on terminal. Any problem for printing character to terminal? 

Thanks,

Jun Zhang

0 件の賞賛
返信

1,817件の閲覧回数
Deeps_bang
Contributor III

Any suggestion to above problem ....??

0 件の賞賛
返信