Support for LPC15xx

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,703件の閲覧回数
johnbatikian
Contributor I

Is there support for the pin config tool for the LPC15xx family particularly the LPC1549?

0 件の賞賛
返信
1 解決策
2,549件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

John Batikian

MCUXpresso doesn't have pin configuration tool for LPC1549.

We can use LPC Initialization instead:

LPC Initialization Tool | NXP 

"The LPC Initialization Tool from NXP® makes it easy for you to create a pin configuration for your target. It generates source code which you can add to yoThe LPC Initialization Tool from NXP® makes it easy for you to create a pin configuration for your target. It generates source code which you can add to your projects"


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

3 返答(返信)
2,550件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

John Batikian

MCUXpresso doesn't have pin configuration tool for LPC1549.

We can use LPC Initialization instead:

LPC Initialization Tool | NXP 

"The LPC Initialization Tool from NXP® makes it easy for you to create a pin configuration for your target. It generates source code which you can add to yoThe LPC Initialization Tool from NXP® makes it easy for you to create a pin configuration for your target. It generates source code which you can add to your projects"


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,549件の閲覧回数
johnbatikian
Contributor I

Thank you. This works! I could not find this from the LPC1549 overview page.

0 件の賞賛
返信
2,549件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 件の賞賛
返信