Support for LPC15xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Support for LPC15xx

Jump to solution
2,736 Views
johnbatikian
Contributor I

Is there support for the pin config tool for the LPC15xx family particularly the LPC1549?

0 Kudos
Reply
1 Solution
2,582 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

John Batikian

MCUXpresso doesn't have pin configuration tool for LPC1549.

We can use LPC Initialization instead:

LPC Initialization Tool | NXP 

"The LPC Initialization Tool from NXP® makes it easy for you to create a pin configuration for your target. It generates source code which you can add to yoThe LPC Initialization Tool from NXP® makes it easy for you to create a pin configuration for your target. It generates source code which you can add to your projects"


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

3 Replies
2,583 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

John Batikian

MCUXpresso doesn't have pin configuration tool for LPC1549.

We can use LPC Initialization instead:

LPC Initialization Tool | NXP 

"The LPC Initialization Tool from NXP® makes it easy for you to create a pin configuration for your target. It generates source code which you can add to yoThe LPC Initialization Tool from NXP® makes it easy for you to create a pin configuration for your target. It generates source code which you can add to your projects"


Have a great day,
Jun Zhang

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

2,582 Views
johnbatikian
Contributor I

Thank you. This works! I could not find this from the LPC1549 overview page.

0 Kudos
Reply
2,582 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

You are welcome!

0 Kudos
Reply