Processor 'MIMXRT1064xxxB' is not supported by MCUXpressoIDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor 'MIMXRT1064xxxB' is not supported by MCUXpressoIDE

ソリューションへジャンプ
1,600件の閲覧回数
chhsu0229
Contributor II

I am working on MIMXRT1064DVL6B processor for develop. The MCUXpressoIDE (v11.9.0_2144) tool does not support it and the message show below,

Capture2.JPG

Capture.JPG

How can I fix this issue? 

0 件の賞賛
返信
1 解決策
1,324件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hello,

Thank you for reporting the problem. Support of MIMXRT1064xxxxB was added and is now available in MCUXpresso Config Tools v15 and Config Tools integrated in MCUXpresso IDE 11.9. 

Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
873件の閲覧回数
JKPAPER_DELOPT_SR
Contributor I

Hello, I am facing a similar problem, I created a custom SDK2_15 for MIMXRTCVJ5B and .mex file. However, the TEE tool is not supported. Also, when I flash the code, it does not retain after Power OFF. I somehow feel that this behaviour is linked to TEE tool enable. Please suggest

 

0 件の賞賛
返信
1,325件の閲覧回数
Lukas_Heczko
NXP Employee
NXP Employee

Hello,

Thank you for reporting the problem. Support of MIMXRT1064xxxxB was added and is now available in MCUXpresso Config Tools v15 and Config Tools integrated in MCUXpresso IDE 11.9. 

Regards,

Lukas

0 件の賞賛
返信
1,551件の閲覧回数
_Leo_
NXP TechSupport
NXP TechSupport

Hi,

Thank you so much for your interest in our products and for using our community.

To work with the MIMXRT1064DVL6B you need to use the SDK_2_15_000_MIMXRT1064xxxxB. Such SDK is supported for the IDE, but at the moment it is not supported for Config Tools. The reason could be that is because is a new silicon revision or a typo. Whatever I already reported to the right department to be corrected in the next revision. Thanks for your feedback.

Meanwhile please take as reference the source code configuration generated by Config Tools for the MIMXRT1064xxxxA.

Hope it helps you.

Have a nice day!

0 件の賞賛
返信
1,345件の閲覧回数
MSchulz
Contributor II

Hi _LEO_,

it's unbelievable!

I also get this error!

HW Revision B of the RT1064 is out now at least more than one year now and there is no Config Tools support yet?

Is there a document describing the differences between REV A and REV B?

Best regards,

Marco.

0 件の賞賛
返信