Hello,
Thank you for reporting the problem. Support of MIMXRT1064xxxxB was added and is now available in MCUXpresso Config Tools v15 and Config Tools integrated in MCUXpresso IDE 11.9.
Regards,
Lukas
Hello, I am facing a similar problem, I created a custom SDK2_15 for MIMXRTCVJ5B and .mex file. However, the TEE tool is not supported. Also, when I flash the code, it does not retain after Power OFF. I somehow feel that this behaviour is linked to TEE tool enable. Please suggest
Hello,
Thank you for reporting the problem. Support of MIMXRT1064xxxxB was added and is now available in MCUXpresso Config Tools v15 and Config Tools integrated in MCUXpresso IDE 11.9.
Regards,
Lukas
Hi,
Thank you so much for your interest in our products and for using our community.
To work with the MIMXRT1064DVL6B you need to use the SDK_2_15_000_MIMXRT1064xxxxB. Such SDK is supported for the IDE, but at the moment it is not supported for Config Tools. The reason could be that is because is a new silicon revision or a typo. Whatever I already reported to the right department to be corrected in the next revision. Thanks for your feedback.
Meanwhile please take as reference the source code configuration generated by Config Tools for the MIMXRT1064xxxxA.
Hope it helps you.
Have a nice day!
Hi _LEO_,
it's unbelievable!
I also get this error!
HW Revision B of the RT1064 is out now at least more than one year now and there is no Config Tools support yet?
Is there a document describing the differences between REV A and REV B?
Best regards,
Marco.