Peripheral not visible in configuration tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Peripheral not visible in configuration tool

8,414 Views
jtro9
Contributor II

MCU: LPC54616J512BD100

IDE: MCUXpresso IDE v10.1.1 [Build 606] [2018-01-02]

SDK: all peripherals and function enable

Problem: In configuration tool -> Peripherals only few peripherals are available (see attachment).

How to see other peripherals as i need to configure CAN, Watchdog, general purpose timer and other.

Kindly guide

10 Replies

7,400 Views
docmo99
Contributor I

Any update for peripherals support in config tools for KL25Z?

 

0 Kudos
Reply

7,309 Views
Lukas_Heczko
NXP Employee
NXP Employee

Hi,

currently there are no plans to support KL25Z in Peripherals tool. As an alternative, I suggest to try KL26Z, which is enabled in Peripherals tool. Sorry for inconveniences caused by leaving KL25Z unsupported. 

Regards,

Lukas 

0 Kudos
Reply

7,771 Views
peoplesurv
Contributor I
0 Kudos
Reply

7,783 Views
marek-trmac
NXP Employee
NXP Employee

Hi jtro9

Peripherals is new tool in Config Tools V4 and it is incrementally added for new devices and peripherals. Currently only first subset is supported. Unfortunately CAN and WatchDog are not supported yet.

Regards

Marek

Regards,
Marek


NOTE: If you find the answer useful, kindly click on [ACCEPT AS SOLUTION] button

7,783 Views
paral_jarek
Contributor I

Hi Marek Trmac‌,

is there any official road map for microcontrollers and peripherals which are going to be available in the module Peripherals (in the Config Tools MCUXpresso)?

I actually would like to use FRDM-KL25Z but the module Peripherals missing in the MCUXpresso.

Best regard
Jarek Páral

0 Kudos
Reply

7,783 Views
Lukas_Heczko
NXP Employee
NXP Employee

Hi Jaroslav,

in the first half of this year we focus on extending MCUXpresso Peripherals tool for LPC processors. We plan to support MCUXpresso Peripherals tool for KL25Z later in Q3 this year.

Hope this information will help you,

Lukas

7,775 Views
tims123
Contributor I

Any Update on availbility?

0 Kudos
Reply

7,783 Views
kurt_staubli
Contributor III

Hi Lukas

What about MCUXpresso Peripherals tool  for MIMXRT1062?

Try to implement something similar to NXP's example evkmimxrt1060_adc_etc_hardware_trigger_conv with Peripherals Tool. Struggle with XBAR. Is it because Peripherals Tool is not yet finished?

Kurt

0 Kudos
Reply

7,783 Views
Lukas_Heczko
NXP Employee
NXP Employee

Hi Kurt,

XBAR is configured by Pins tool. 

Specifically for use case from evkmimxrt1060_adc_etc_hardware_trigger_conv example where XBAR is configured to trigger ADC ETC from PIT Channel 0, you can set this in Pins tool following way: in Peripherals Signals tab expand ADC_ETC list and enable XBAR0_TRIG 0. In window with signals that can be routed to the ADC_ETC XBAR trigger 0 pick PIT_TRIGGER0. 

Hope this will help,

Lukas

0 Kudos
Reply

7,783 Views
jtro9
Contributor II

Thanks Marek Trmac for update

I hope all peripherals will come in config tool soon...

0 Kudos
Reply