MKV42F256xxx16 maximum clock frequency?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKV42F256xxx16 maximum clock frequency?

Jump to solution
4,082 Views
andreipalamarci
Contributor I

Hello.

I'm working with MKV42F256VLH16 and i'm trying to configure the clock frequency as higher as possible.

As per datasheet it should be possibile to configure the clock up to 168MHz but the MCUXpresso Config Tools v4.1 limit it to 100MHz.

nxp_frequency_constraint.png

Is this a MCUXpresso Config Tools v4.1 issue or a MKV42F256xxx16 issue?

Thank you for helping.

Labels (1)
1 Solution
3,941 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andrei Palamarciuc ,

In HSRUN mode , can configure  core clock to highest 168MHZ:

pastedImage_2.png

Please see data sheet, in Normal run mode , the Max core clock is 100MHZ.

pastedImage_4.png

Hope it helps,


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
3,942 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Andrei Palamarciuc ,

In HSRUN mode , can configure  core clock to highest 168MHZ:

pastedImage_2.png

Please see data sheet, in Normal run mode , the Max core clock is 100MHZ.

pastedImage_4.png

Hope it helps,


Have a great day,
Alice

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------